Skip to main content
Pasi MYLLYMAKI
ST Employee
May 11, 2020
Question

Question from Predictive Maintenance Webinar 29th of April: Can we measure electrical signature using magnetometer in STWIN kit?

..

    This topic has been closed for replies.

    1 reply

    Vladimir JANOUSEK_34072
    Visitor II
    May 13, 2020

    Yes, this is possible. IIS2MDC is potentially the product which can be considered. It Is important to respect the magnetic field strenght vs. IIS2MDC measurement range, and if the sampling speed is sufficient for particular application (150Hz max) etc.