Skip to main content
Pasi MYLLYMAKI
ST Employee
May 11, 2020
Question

Question from Predictive Maintenance Webinar 29th of April: Can I use the IIS3WB with the X-Nucleo -IKSS01A3?

..

    This topic has been closed for replies.

    1 reply

    Vladimir JANOUSEK_34072
    Visitor II
    May 13, 2020

    Yes it is possible, but you have to change IKS01A3 communication from default I2C to SPI (for the DIL24 socket at IKS01A3), then connection of STEVAL-MKI208V1K is possible. Currently there is no out of the box SW project published to suport this combination of HW, but there are many source codes available which could be adapted. For example to look at X-CUBE-MEMS1 SW package as starting point for IKS01A3 in general.