Skip to main content
Explorer
June 11, 2024
Solved

Question for LPS25HB Pin#7 connection

  • June 11, 2024
  • 1 reply
  • 921 views

I am designing to mount LPS25HB on the board.

Communication is I2C.

Please help me with the connection of Pin 7 (INT_DRDY).
Is this pin an open pad? Or does it need to be connected to GND?

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @genki ,

Welcome to ST Community!

INT_DRDY pin is an output of the device. If not used can be left floating. In other case it must be connected to GPIO of microcontroller to verify the features of this pin (see page 37 of LPS25HB datasheet)

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
June 11, 2024

Hi @genki ,

Welcome to ST Community!

INT_DRDY pin is an output of the device. If not used can be left floating. In other case it must be connected to GPIO of microcontroller to verify the features of this pin (see page 37 of LPS25HB datasheet)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.