Skip to main content
Visitor II
Oct 19, 2026 3:16 AM UTC
Question

Question about MLC output latency on the LSM6DSV16X

Hi everyone,

We’re currently evaluating the LSM6DSV16X for a multimodal data acquisition application and are using its Machine Learning Core (MLC) to detect specific events and generate corresponding labels in a time-series data stream.

To ensure accurate temporal alignment between different data sources, we’d like to understand the latency between the actual occurrence of a physical event and the availability of the corresponding MLC output.

Has ST characterized this latency or published any relevant specifications, test results, or documentation? If not, is there a recommended test procedure or validation methodology for measuring it reliably?

Any insights or suggestions from the ST team or community members with experience using the MLC would be greatly appreciated.

Thanks in advance for your help!

1 reply

Federica Bossi
ST Technical Moderator
Oct 29, 2026 1:22 PM UTC

Hi ​@Annika Jiang 

ST does not specify an end-to-end latency from the physical onset of an event to the availability of the corresponding MLC classification.

However I can share some useful information: an MLC result is stored in the FIFO when the corresponding MLCx_SRC value changes, and the FIFO entry includes a timestamp. Windowed MLC features are stored at the end of each window; filters and recursive features are stored at the configured MLC output data rate.

The device timestamp has a nominal resolution of 21.7 μs, but this is timestamp resolution, not MLC detection latency.

For an application-specific measurement, use a repeatable stimulus with a measurable reference onset, capture that reference alongside the MLC interrupt or FIFO result, and calculate the latency over repeated trials. It is important to include the MLC configuration, sensor ODR, filter settings, and feature-window length, and to vary the event’s timing relative to the sensor sampling period. This will help quantify both the average latency and its variation.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.