Skip to main content
avieira
Associate
February 12, 2014
Question

Question about LIS3DH FIFO

Posted on February 12, 2014 at 17:44

Hello

I am trying to use the LIS3DH in FIFO Mode with Filter enabled.

In this mode, the X-Axis, and Y-Axis values get some normal values (they oscillate between -10 and +10) but the Z-Axis value seems to have a bypass to the filter mode, the Z-Axis gives for example -616 witch is not the value for Z-Axis if i disable FIFO and Filter.

Is this some kind of limitation of LIS3DH? or am i making something wrong at initialization.

In my initialization code the registers are initialized with the following values:

CTRL_REG1 = 0x17

CTRL_REG2 = 0x88

CTRL_REG3 = 0x00

CTRL_REG4 = 0x40

CTRL_REG5 = 0x40

CTRL_REG6 = 0x00

FIFO_CTRL_REG = 0x40

Thank You

Artur Vieira

This topic has been closed for replies.

5 replies

bw_it
Associate
February 19, 2014
Posted on February 19, 2014 at 10:31

Hi,

There seem to bee a limitation in LIS3DH regarding using FIFO, HP-FILTER and the Z-axis

even though

it is not documented (yet?). The reply I got from the support team was that if this functionality was require the they suggested using the LIS2DH.

avieira
avieiraAuthor
Associate
February 19, 2014
Posted on February 19, 2014 at 18:28

Hello

thanks for the feedback.

There i go redesign the PCB, since the footprint is not the same between LIS2D and LIS3D.

thanks

bw_it
Associate
February 20, 2014
Posted on February 20, 2014 at 09:55

Please notice that I have not yet worked with the LIS2DH, and can there for not confirm that the HP+FIFO configuration actual works on the Z-axis, and can't find and other source of confirmation on this.

avieira
avieiraAuthor
Associate
February 20, 2014
Posted on February 20, 2014 at 12:21

Hi

I have asked to my local ST distributor if the LIS2DH has any problem for this kind of application.

I am waiting for his confirmation.

Thanks 

avieira
avieiraAuthor
Associate
February 21, 2014
Posted on February 21, 2014 at 10:27

Hi

Just to update.

I get the confirmation from ST that there is a problem with LIS3DH when using FIFO + HP-Filter and Z-Axis.

Also get the confirmation, that LIS2 does not suffer from this problem.