Skip to main content
rahul23
Associate
October 23, 2015
Question

Query regarding IMU sensor for Golf Swing Analyses

Posted on October 23, 2015 at 08:33

I am in search of 6 or 9 axis IMU mems sensor for golf swing analyses device.

The device would be somewhat like  http://3bayslife.com/zone-1/ 

Should I go for 6 axis DOF or 9 axis DOF? Low power operation is must. 

Also the captured data is to be transmitted via bluetooth to smartphone. 

Suggest me with suitable options for 6 or 9 axis MEMs (which one is better and why?) and also the bluetooth socs that are suitable for this project.

#golf-swing-analyses
This topic has been closed for replies.

3 replies

rahul23
rahul23Author
Associate
October 29, 2015
Posted on October 29, 2015 at 08:56

Unfortunately, I do not see any replies coming. 

This is my first post on ST community. 

oyvind2
Visitor II
October 29, 2015
Posted on October 29, 2015 at 09:53

Unfortunately, this forum is not very useful. Perhaps you should try invensense or bosch.

Visitor II
March 26, 2024

I also need a device to analyze the golf swing so I can video it and put it on YouTube. Where can I get this device?