Skip to main content
RWasw.1
Associate
July 4, 2022
Question

Query about LSM6DSR read/write address on I2c interface

I am using LSM6DSR on I2c interface. As per datasheet when the SDO/SAO pin of the sensor is connected to ground the read/write address should be D5H/D4H but currently the read/write address is D7H/D6H. Can you please explain the reason for this? Has anyone experienced this issue before?

    This topic has been closed for replies.

    5 replies

    Eleon BORLINI
    ST Employee
    July 8, 2022

    Hi @RWasw.1​ ,

    can you check your schematic to validate that the SDO/SA0 pin is at the correct voltage level?

    In any case, is this issue impacting the correct functioning of your application (in term of data acquisition / current consumption)?

    -Eleon

    RWasw.1
    RWasw.1Author
    Associate
    July 11, 2022

    Hi @Eleon BORLINI​ ,

    We have checked the voltage at this pin and it is at low level.

    This is not affecting the data acquisition/current consumption but we have concern that we should not have this addressing issues during mass production because we are looking towards the root cause and until now we haven't found any.

    -Ravi

    Eleon BORLINI
    ST Employee
    July 18, 2022

    Hi Ravi @RWasw.1​ ,

    understood.

    How many devices did you tested showing this behavior?

    -Eleon

    RWasw.1
    RWasw.1Author
    Associate
    July 19, 2022

    Hi @Eleon BORLINI (ST Employee)​ ,

    We have tested on 2 devices and both of them show the same behaviour.

    -Ravi

    Visitor II
    June 18, 2023

    If you're seeing the address 0xD7 when you connect the SDO/SAO pin to ground, it probably means that the sensor is set to use a newer communication mode called I3C.
    To get things back to normal and disable I3C mode, you have a couple of options:

    1. Connect a pull-down resistor to the INT1 pin of the sensor. This basically tells the sensor to chill out and go back to regular I2C mode.

    2. Send a software command to the sensor to turn off I3C mode. It's like giving the sensor a little digital nudge to make it behave and go back to its regular I2C ways.