Skip to main content
LRoss.1
Visitor II
March 20, 2020
Question

Quaternions in AlgoBuilder with sensortile box

Hi everyone,

I'm using the quaternions and the sensor fusion in Algobuilder with the Sensortile box in order to compare the signal of the quaternions and the position of the teapot, but I don't understand the relation between both of them... Any idea?

When I turn the Sensortile box 90° in X-axis, the teapot turns -90°.... WHY???

Thanks!

This topic has been closed for replies.

1 reply

RMcCa
Senior II
March 20, 2020

"Conpare the signal of the quaternions And the position of the teapot"

​

When did Lewis Carroll start writing code?​

​