Skip to main content
bassem.saleh93
Associate II
Jul 28, 2019 9:51 AM UTC
Solved

Problem with L3G4200 Sensor using I2C

I have a problem interfacing with L3G4200 using I2C on STM32F469 Discovery. Here is my code to config the I2C

void I2CConfig(void){
	I2CHandle1.Instance = I2Cx;
	I2CHandle1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
	I2CHandle1.Init.ClockSpeed = 100000;
	I2CHandle1.Init.DutyCycle = I2C_DUTYCYCLE_2;
	I2CHandle1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
	I2CHandle1.Init.OwnAddress1 = 0xD0;
	I2CHandle1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
	I2CHandle1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
	if (HAL_I2C_Init(&I2CHandle1) != HAL_OK)
		Error_Handler();
}

And here is the code to initialize the I2C on HAL_Init file

void HAL_I2C_MspInit(I2C_HandleTypeDef *hi2c){
	GPIO_InitTypeDef GPIO_InitStruct;
 
	/*##-1- Enable peripherals and GPIO Clocks #################################*/
	/* Enable GPIO TX/RX clock */
	I2Cx_SCL_GPIO_CLK_ENABLE();
	I2Cx_SDA_GPIO_CLK_ENABLE();
	/* Enable I2Cx clock */
	I2Cx_CLK_ENABLE();
 
	/*##-2- Configure peripheral GPIO ##########################################*/
	/* I2C TX GPIO pin configuration */
	GPIO_InitStruct.Pin = I2Cx_SCL_PIN;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull	 =	GPIO_PULLUP;
	GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
	GPIO_InitStruct.Alternate = I2Cx_SCL_SDA_AF;
	HAL_GPIO_Init(I2Cx_SCL_GPIO_PORT, &GPIO_InitStruct);
 
	/* I2C RX GPIO pin configuration */
	GPIO_InitStruct.Pin = I2Cx_SDA_PIN;
	GPIO_InitStruct.Alternate = I2Cx_SCL_SDA_AF;
	HAL_GPIO_Init(I2Cx_SDA_GPIO_PORT, &GPIO_InitStruct);
}

I can't figure out where is the problem because I successfully interfaced i2c using another sensor (BMP180) and also interfaced SPI with the L3G4200 with the same board.

This topic has been closed for replies.
Winfred LU
Winfred LUBest answer
ST Employee
Jul 29, 2019 8:10 AM UTC

Hi,

I2C is an open drain interface, neither the master nor the slave shall pull the bits high.

External pull-up resistors are required for both I2C clock and data pins. The pins can only be pulled down when needed.

So, please instead use:

GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull	 = GPIO_NOPULL;

Best Regards,

Winfred

1 reply

Winfred LU
Winfred LUBest answer
ST Employee
Jul 29, 2019 8:10 AM UTC

Hi,

I2C is an open drain interface, neither the master nor the slave shall pull the bits high.

External pull-up resistors are required for both I2C clock and data pins. The pins can only be pulled down when needed.

So, please instead use:

GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull	 = GPIO_NOPULL;

Best Regards,

Winfred