Skip to main content
apenn.13
Associate III
December 13, 2019
Question

Problem with Bluecoin and echo cancellation

Hy,

I'm trying to do some tests on echo suppression using evaluation boards BlueCoin and CoinStation.

The software I use is the one provided by ST to interact with BlueCoin that is, FP-"AUD-SMARTMIC1 GUI.exe" in addition to the

audacity.exe program.

As specified in the document , "Getting started with STM32Cube function pack for MEMS microphones acquisition, advanced audio

processing and audio output" (UM2219) paragraph 4.5, I would expect to hear on the output left only the signal picked up by

the microphone while on the right output the microphone signal plus the audio fragment.

I actually hear the microphone signal plus the audio fragment on both output left and right.

What should I do to hear on the output left only the microphone (and then have the proof that the echo cancellation worked) ?

The program loaded on the board BlueCoin is the version 1.0.0 ( Device presentation string: OSX SMARTMIC1 | BlueCoin Dev Kit |Embedded Microphones|1.0.0)

Thank you

    This topic has been closed for replies.

    4 replies

    Eleon BORLINI
    ST Employee
    December 16, 2019

    Hi @apenn.13​ , to answer your question:

    >> What should I do to hear on the output left only the microphone (and then have the proof that the echo cancellation worked)?

    when the AEC feature is active, the "audio out" sends only the audio fragment, not the microphone, which is then cancelled by the AEC itself.

    To check it is well working, you have to acquire the stream via USB and check if the audio fragment has been cancelled.

    Regards

    apenn.13
    apenn.13Author
    Associate III
    December 16, 2019

    Hi,

    thank you your answer.

    My application also includes a low-cost product and I saw that echo canceller runs on the whole STM32F4 family. Can I also use 48-pin STM32F410CBT or 32K of ram is little? Are the necessary mips okay? The alternative would be STM32F401 but is it 64 pin?

    Regards

    Eleon BORLINI
    ST Employee
    January 8, 2020

    Hi @apenn.13​ , sorry for the late answer. It is better to use at least an STM32F401RE, if it is not possible to use the Bluecoin STM32F446 180 MHz MCU. The HAL drivers are the same for the entire STM32F4xx, so you can try to run the same libraries on the STM32F410 (paying attention to the pin connections), but I cannot guarantee you the same performances / latency... Regards

    apenn.13
    apenn.13Author
    Associate III
    March 4, 2020

    Hi,

    I tried echo cancellation with the bluecoin evaluation card and the SMARTMIC1 V2.0.0 application.

    Everything seems to be working properly.

    Now I would like to implement the echo deletion procedure on our card using the micro stm32f401re

    and a mems microphone at a sampling rate of 8khz.

    I wrote some code using the evaluation card stm32nucleo that mounts the micro stm32f401re since still our hw is not ready.

    I realized that the execution of the process AcousticEC_Process that runs inside a low priority interrupt lasts about 8 msec

    while in the bluecoin board that mounts a stm32f446 lasted about 300 usec.

    The difference in process execution time seems to me to be excessive.

    I would have expected a doubling of the time or a little more, since the micro works at 84 MHz while in the bluecoin it works at 168 MHz and

    assuming that the dsp has the same characteristics in both cases.

    Is there an explanation for this ?

    Regards