Visitor II
January 27, 2017
Question
Problem reading value gyroscope
- 0 replies
- 579 views
Posted on January 27, 2017 at 15:04
Hello, sorry for me level in English
I have to carry out an end of year project of electronic bts, and I am stuck at this level
I need your help to understand a lack of reading in the following code
I use this soft : 'Sensors_Reader', it is a program provided on the page of the site MBED
I have this board NUCLEO_L476RG and this shield sensors 'X-NUCLEO-IKS01A1'
I receive this information in return on 'un moniteur serie' :
--- Starting new run ---
Humidity | Temperature Sensor ID = HTS221 (0xbc | 0xbc)Gyroscope | Motion Sensor ID = UNKNOWN (0x0 | 0x0)===I2C [errors]: 0x00 X Y ZMAG [mgauss]: 0 536872992 214ACC [mg]: 0 0 134247283GYR [mdps]: 0 0 5---TEMP | HUMIDITY: 27.54°C | 25.72%TEMP | PRESSURE: 0.00°F | 0.00mbar
===The problem is that I do not have the pressure values, can you help me to fix this problem
I have attached the contents of the program
#x-nucleo-iks01a2 #lps22hb