Skip to main content
Associate III
Sep 2, 2025 5:57 AM UTC
Solved

Order of operation of INT2_CTRL (0Eh) in ASM330LHH

Should INT2_CTRL (0Eh) in ASM330LHH be changed when ODR_XL[3:0] in CTRL1_XL is 0, or should it be changed after being set to non-zero?

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Sep 11, 2025 12:26 PM UTC

Hi @ggob ,

It is recommended to configure INT2_CTRL only after enabling the accelerometer with a non-zero ODR.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Sep 11, 2025 12:26 PM UTC

Hi @ggob ,

It is recommended to configure INT2_CTRL only after enabling the accelerometer with a non-zero ODR.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.