Skip to main content
Hicss.2033
Associate III
October 17, 2019
Question

On a STM32F429I discovery, also when the board is not moving, the gyroscope furnish values different from zero and with high variance (on all the three axes). Is this noise or sensitivity? Is it possible to utilize some filter?

..

    This topic has been closed for replies.

    3 replies

    Eleon BORLINI
    ST Employee
    October 18, 2019

    Hi @Hicss.2033​ , it is normal to get values different from 000h. If you consider the L3GD20 gyro (the sensor mounted on that discovery board), which is btw an old part number, the zero rate level is:

    0690X00000AqYLqQAN.png

    while the sensitivity is 8.75mdps/LSB in case of FS +-200dps.

    So the ouptut gyro can be a value between +-477h (decimal -+10/0.00845 LSB). Is this your case?

    Regards

    Hicss.2033
    Associate III
    June 8, 2020

    Also I see that there is drift whenutilizing the gyroscope. Is it possible to eliminate such drift?

    Hicss.2033
    Associate III
    June 8, 2020

    Sorry for the late replay, but when I'm rotating the board, does the digital zero rate level must be considered to get the speed of rotation of the board (for example the speed of rotation is the measured value +- the digital zero rate level)? Is there some technique that I must adopt to get such measure or some technical notes that explain how to get such measure? thanks for yor answer.