Skip to main content
Visitor II
Jul 21, 2025 8:36 AM UTC
Question

Negative X-Axis Clipping on IIS3DWB When Stationary

Dear All,

We are using the IIS3DWB MEMS accelerometer in one of our products and have encountered an issue with a single unit that we would like your input on.

 

Issue description:

On this specific device, the X-axis always reports the maximum negative value (−32768 in 2’s complement), regardless of the selected full-scale range or output data rate. The Y and Z axes function correctly. The issue persists across power cycles and register resets and started after using it for 6-8 months.

 

We have verified the following:

• The offset registers are set to 0.

• No filters or self-test modes are enabled.

• The axis is properly enabled.

• The unit was removed from its casing to exclude mechanical stress.

• This appears to be a one-off issue; all other units from the same batch are functioning normally.

 

We would appreciate your insights on what might cause this axis-specific saturation behavior and whether there are diagnostic procedures or failure analysis options you recommend.

 

Kind regards,

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
Jul 23, 2025 9:42 AM UTC

Hi @stBob ,

What kind of tests did you perform on this piece? It appears to have been damaged by some stressful event.

Can you please run the self-test procedure as described in AN5444, Section 8? Otherwise, you can follow the example on Github

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.