Skip to main content
ChawCS
Associate
August 3, 2020
Question

Movement of a device in XY.

I had a device that need to record data then plot the location. What type of mems sensor should I use?

Will it give the location or just reference.

CS

    This topic has been closed for replies.

    3 replies

    niccolò
    ST Employee
    August 7, 2020

    Hi @ChawCS​ ,

    the state of the art for plotting the location of a device make use of GPS modules because MEMS motion sensors are not able to provide data that can be analysed to plot a position in a 2/3D environment with enough accuracy.

    Anyway, if you would like to research how accurate the plot from MEMS sensors data can be, you can try any accelerometer, like LIS2DW12, or even a 6-axis module, that can help with gyroscope data, like LSM6DSOX.

    does this help you?

    Niccolò

    ChawCS
    ChawCSAuthor
    Associate
    August 8, 2020

    Hi Niccolo,

    As this device (mobile car) will be in-house, do you think GPS can do the job?

    Think a reference distance will do, mean the device move left, right. As it is to guide a curve line, as in a circle.

    Regards

    ChawCS

    niccolò
    ST Employee
    August 10, 2020

    Hi @ChawCS​,

    I did not kept into consideration the distances you have to work with. for a precise positioning of this kind I don't think GPS is suitable.

    So I would try to use a LSM6DSOX (6-axis module) to try to solve this problem. Maybe you will not have a perfect positioning, but, with the right references around the device, it can be done.