Skip to main content
Associate
August 6, 2024
Solved

MotionMC_initialize() with ARM M33 is hard floating point is leading into a infinite loop

I tried to set up a project and to do the calibration of the sensor IIS2MDC on my B-U585I-IOT02A Board I want to use MotionMC

Now the floating-point-ABI ist set to Hardware implementation and the Middleware used is the MotionMC Library MotionMC_CM33F_wc32_ot_hard.a

 

But when I use the function MotionMC_Initialize(sampletime, enable) it ends up in an infinite loop.

 

What solutions could I try to solve this?

This topic has been closed for replies.
nedpavelBest answer
Associate
August 6, 2024

Enabling the CRC Clock with one line inside MX_CRC_Init() befor the use of MotionMC_Initialize was enough:

__HAL_RCC_CRC_CLK_ENABLE();

 

B

1 reply

nedpavelAuthorBest answer
Associate
August 6, 2024

Enabling the CRC Clock with one line inside MX_CRC_Init() befor the use of MotionMC_Initialize was enough:

__HAL_RCC_CRC_CLK_ENABLE();

 

B