Skip to main content
N ORhan
Associate III
Jan 16, 2020 10:21 AM UTC
Solved

MotionGC Init and SetFrequency Funcitons

Hi everyone. I'm using MotionGC library to calibrate my LSM6DSL gyroscope. In User Manual of library it is stated that "void MotionGC_Initialize(float freq) "function takes "float" as input argument. But when I call the function according to the user manual, I got a Hard Fault. If I pass the frequency variable input as its address and define Init function as "void MotionGC_Initialize(float *freq)" no faults observed, it looks like it works but I can not be sure if its working properly. Calibration process takes much time.

Is there anyone who had any experience about this problem?

Thanks.

    This topic has been closed for replies.
    Miroslav BATEKBest answer
    ST Employee
    Jan 16, 2020 11:07 AM UTC

    Hi @Nazım Önder ORhan​

    you have to pass the freq value as pointer (address). There is a bug in the User Manual.

    The device must be still to get the calibration values. You can fine tune the knobs to have faster convergence but less accuracy.

    2 replies

    Miroslav BATEKBest answer
    ST Employee
    Jan 16, 2020 11:07 AM UTC

    Hi @Nazım Önder ORhan​

    you have to pass the freq value as pointer (address). There is a bug in the User Manual.

    The device must be still to get the calibration values. You can fine tune the knobs to have faster convergence but less accuracy.

    N ORhan
    N ORhanAuthor
    Associate III
    Jan 16, 2020 2:25 PM UTC

    Thanks Mr Batek.