Skip to main content
Pajaka
Associate III
June 30, 2022
Question

MotionFX yaw problem

Hi, I use LSM9DS1 in my project. I also use MotionMC and MotionFX libraries to calibrate the magnetometer and fuse data respectively and I have a following problem regarding the yaw output. The roll and pitch work flawlesly but the yaw output reading gets stuck - it does not respond to any movement unless I apply some amount of acceleration to the board. Slight tapping usually forces the yaw to update to somewhat correct orientation. What can I do about it? I first perform mag calibration until the CalQuality is equal to MMC_CALQSTATUSGOOD. Then I apply the hard bias as well as rotation matrix before updating the Kalman filter from the MotionFX lib. The ACC/Gyr ODR is 119Hz, magnetometer 80Hz. I also perform mag calibration once every few samples online. I also found out the calibration does not work when the mag ODR is bigger than 80 Hz for some reason - the CalQuality is always MMC_CALQSTATUSUNKNOWN.

    This topic has been closed for replies.

    2 replies

    Martin B
    ST Employee
    July 19, 2022

    Can you share algorithms input (sensor) data and related algorithms output data to be able to replicate issue, please?

    Pajaka
    PajakaAuthor
    Associate III
    January 31, 2023

    Sorry for my inactivity. I managed to get it working.