Skip to main content
Yong Cai
Associate
October 11, 2017
Question

MotionFX Initialization Failed

Posted on October 11, 2017 at 10:55

Hello,

I'm a noob on stm32 and keil, I'm not sure the problem is my operation in keil or my configuration about stm32 and x-cube-mems1. Please help with the details.

I successfully run the DataLogFusion example in Nucleo-F401RE and X-NUCLEO-IKS01A2. But when I try to use MotionFX lib in my custom board project, I get this issue.

In debug session, the program could not STEP OVER the function - MotionFX_initialize().

Using

1. Custom board using STM32F401CEUx

2. MotionFX V2.0.0, included MotionFX200_CM4F_Keil_ot.lib

3. Code generated by STM32 CubeMX 4.22, STM32Cube FW_F4 V1.16.0

    This topic has been closed for replies.

    8 replies

    ST Employee
    October 11, 2017
    Posted on October 11, 2017 at 11:00

    Hello,

    please enable clock for CRC unit in the microcontroller, it is needed for the algorithm initialization.

    Yong Cai
    Yong CaiAuthor
    Associate
    October 11, 2017
    Posted on October 11, 2017 at 11:56

    Yes, it works by adding __CRC_CLK_ENABLE();