Skip to main content
Visitor II
May 28, 2024
Question

MotionFx ATime, MTime and FrTime Parameter

I'm currently trying to stabilize the MotionFx Sensorfusion in an environment with medium magnetic disturbances. However I don't quite understand the three parameters ATime, MTime and FrTime from the Knobs structure. For example the manual UM2220 describes the values in a range from 0 to 1 but the default value in the startup seems to be 1.5f for the the MTime Parameter.

So from UM2220 I deduct that MTime and FrTime should be at a high value near 1 (e.g. 0.95f), but I don't experience a major change setting those parameters accordringly. So what is the correct range for the parameters and how do I set them, if I want my transfer function to be stable against low magnetic disturbances? Thanks in advance! I'm using version 2.7.1 btw.

Moritz

This topic has been closed for replies.