Skip to main content
Visitor II
May 24, 2024
Solved

Minimum RAM required warning

Hi, I am working on Anomaly Detection in motor using ISM330ISN. As soon as I am choosing the Buffer Size of 256 in the datalogger and adding the signal, I am getting this warning of minimum RAM required is 9KB. However upto 128 buffer size, it is working fine. What is the reason that I am getting warning as I am going above 128 buffer size ? @Denise SANFILIPPO @Eleon BORLINI 

jayantver_0-1716554438620.png

 

 

This topic has been closed for replies.
Christian N
Christian NBest answer
ST Employee
May 28, 2024

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

2 replies

Federica Bossi
ST Technical Moderator
May 28, 2024

Hi @jayant-ver ,

Welcome to ST Community!

From 128 to 256 doubles the size of the sample buffer, so memory occupancy goes up, and with 256 it rises above the maximum 8K.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Christian N
Christian NBest answer
ST Employee
May 28, 2024

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.