Skip to main content
LPetr.1
Senior
Apr 22, 2026 6:14 AM UTC
Question

MEMS Studio weird behaviour

I am using MEMS Studio to evaluate FSM and MLC on the STEVAL-MKI109D + STEVAL-MKI238A . I noticed few strange things. I am attaching my FSM gui config and reg config (config.zip)

1. When I open the FSM tab and load the state machine files and device configuration file

LPetr1_0-1776837341168.png


one thing I notice right away that its not loading the Long Counter Max value correctly.
In my saved FSM configuration I have set it to 0x14 but when I load the configuration it still showing up at 0001

LPetr1_1-1776837477540.png


Now when I click "Write FSM configuration to the sensor" button and head to Register Map tab, I do see 0x14

LPetr1_2-1776837555092.png



This is very misleading as the FSM configuration tab is different value that is actually written to registers.

 

 

2. Next thing I notice is that when I load my FSM configuration and GUI files and click "Write FSM configuration to the sensor". Head to Sensor Evaluation and return back to Advanced features -> FSM. The FSM ODR now changes to 12.5 Hz.

This is how FSM tab looks when I load gui and config files but before writing config to sensor:

LPetr1_4-1776837837137.png

 

And this is how it looks after writing config to sensor, clicking Sensor Evaluation and returning to Advanced Features -> FSM

LPetr1_5-1776838014571.png

 

Why would the ODR change when leaving the FSM tab and returning back to it?

 

3. I want to clarify if I must have STOP (0x0D) command on my FSM? I notice that if I don't add STOP command in my FSM and click "Write FSM configuration to sensor" I see that STOP command is automatically appended into my FSM. Is that expected behaviour?


 

4. I was further playing around and testing with the FSM and came up with 3 FSM's. See attached FSM_crashing.zip

When I click "Write FSM configuration to the sensor" the application crashes and hangs on this screen:

LPetr1_6-1776838441798.png

Im sure I have misconfigured the FSM somehow but it would be nice if MEMS Studio would not crash/hang and instead tell me that something is wrong.



1 reply

Federica Bossi
ST Technical Moderator
Apr 28, 2026 2:47 PM UTC

Hi @LPetr.1 ,

Thank you for feedback, we reviewed your issues. We will provide our response for each item:

1-2) We identified a visualization issue which will be fixed in next release of MEMS Studio

3) The FSM size should be always even. If requested configuration size is odd MEMS Studio will automatically ad an extra STOP command in order to get an even size.

4) The configuration generated was not processed properly, next MEMS Studio release will resolve this issue.

Best regards

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.