Skip to main content
Visitor
Jul 16, 2026 6:40 AM UTC
Solved

MEMS Studio — "Quick Setup" missing for X-NUCLEO-IKS02A1 on NUCLEO-F401RE

Hi,

NUCLEO-F401RE + X-NUCLEO-IKS02A1, MEMS Studio v2.4.0. Flashed DataLogFusion (Applications\IKS02A1\DataLogFusion), connects fine (X-NUCLEO-IKS02A1, FW: 12.1.0), but I only get "Library Evaluation" (Data Table, Charts, Sensor Fusion...). No "Quick Setup" / "Sensor Evaluation" anywhere, including under Advanced Features. DataLogTerminal gives "Board not identified."

An older tutorial (MEMS Studio v1.3.0) shows a "Sensor Evaluation" section with Quick Setup, Registers Map, FSM, MLC, Qvar — raw register access, not fusion output.

Question: Which X-CUBE-MEMS1 firmware (if any) enables "Sensor Evaluation"/"Quick Setup" for this board combo? Is it firmware-specific or was it removed in MEMS Studio v2.x?

Thanks!

Miroslav BATEKBest answer
ST Employee
Jul 16, 2026 11:46 AM UTC

Hello,

Applications like DataLogFusion do not expose the Quick Setup page in MEMS Studio because the sensor configuration is hardcoded in the firmware.

For sensor evaluation, you need the DatalogExtended firmware. This firmware has been moved from the X-CUBE-MEMS1 package to MEMS Studio. X-NUCLEO-IKS02A1 has now been replaced by X-NUCLEO-IKS5A1 and will be deprecated soon, so DatalogExtended for this board is not available in MEMS Studio nor in the latest version of X-CUBE-MEMS1.

The last version of X-CUBE-MEMS1 where you can find DatalogExtended for X-NUCLEO-IKS02A1 is v12.0.0. You can download it from here.

2 replies

Miroslav BATEKBest answer
ST Employee
Jul 16, 2026 11:46 AM UTC

Hello,

Applications like DataLogFusion do not expose the Quick Setup page in MEMS Studio because the sensor configuration is hardcoded in the firmware.

For sensor evaluation, you need the DatalogExtended firmware. This firmware has been moved from the X-CUBE-MEMS1 package to MEMS Studio. X-NUCLEO-IKS02A1 has now been replaced by X-NUCLEO-IKS5A1 and will be deprecated soon, so DatalogExtended for this board is not available in MEMS Studio nor in the latest version of X-CUBE-MEMS1.

The last version of X-CUBE-MEMS1 where you can find DatalogExtended for X-NUCLEO-IKS02A1 is v12.0.0. You can download it from here.

netanbiAuthor
Visitor
Jul 16, 2026 12:16 PM UTC

thanks!!!! for correction only in 11.3 it works