Skip to main content
Visitor
Oct 23, 2026 2:27 AM UTC
Question

MEMS Studio protocol support for a custom STM32C5A3 board

Hello ST Support Team,

We are developing a custom evaluation board using the STM32C5A3REG6 MCU and ISM330DHCX IMU.

We would like to connect our board directly to MEMS Studio via USB without using the STEVAL-MKI109D motherboard.

We have reviewed UM3420 and UM3233, but would like to clarify the following:

  1. Can MEMS Studio recognize a custom STM32-based board?

  2. Is implementing the ProfiMEMS serial command protocol sufficient?

  3. Does MEMS Studio require specific USB VID/PID values, board identification commands, or firmware version responses?

  4. Is the complete communication protocol or compatible firmware source code available?

  5. Can the MLC configuration, training workflow, and sensor data visualization functions be used with custom hardware?

Thank you.

1 reply

Federica Bossi
ST Technical Moderator
Nov 10, 2026 11:32 AM UTC

Hi ​@yunjun ,

Yes, a custom board can be interfaced with MEMS Studio by implementing the ProfiMEMS compatible communication protocol in its firmware. The board must handle the expected commands and return responses and sensor data using the same structure and format as ProfiMEMS.

Please use the protocol description in the ProfiMEMS user manual as a reference and adapt it to your hardware.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.