Skip to main content
Associate II
Aug 31, 2026 3:20 PM UTC
Solved

MEMS Studio: NUCLEO-F401RE + X-NUCLEO-IKS5A1 "board not identified"

Hello, I would like to use a magnetometer to develop a small system that can discern the presence of a certain object with a magnet mounted on top of it. For this reason I got a X-NUCLEO-IKS5A1 as a starting point.

From my understanding the faster approach was to connect the NUCLEO board NUCLEO-F401RE (which I already had) to the aforementioned X-NUCLEO board with the software MEMS-Studio.

So I followed the procedure explained here:
 

 

and applied it to the “new” X-NUCLEO -IKS5A1 board (instead of the IKS4A1 described in the video).

I’ve successfully programmed the board with the supplied firmware (STMicroelectronics/MEMS Studio/firmware/mems-studio/x-nucleo-iks5a1/nucleo-f401re/DataLogExtended.bin, Interface MASS STORAGE, Device_ NODE_F401RE).

But when I try to connect the board it says:

And I cannot go further with the procedure.

Is there something wrong with my procedure? Any idea of the issue?

If not, how can I start using this board? Starting from an STM32CubeMX project?

Thank you for your support,

Regards,

M.

MCA_DevBest answer
Associate II
Sep 9, 2026 8:05 AM UTC

Hello, thank you for your feedback.

Yes, it was indeed a connection problem, I was able to communicate directly with the sensor via I2C (with a test FW) but not through the serial port. I discovered that the NUCLEO-F401RE did not have the configuration 0R resistors SB14 and SB13 mounted so it was impossible to use the main serial communication used by MEMS Studio.

Regards,

2 replies

Federica Bossi
ST Technical Moderator
Sep 1, 2026 2:09 PM UTC

Hi ​@MCA_Dev ,

It seems that the issue may be related to the connection/interface selection rather than the programming step itself.

Please try the following:

  1. Program the board using the ST-LINK interface

  2. Check the correct COM por

  3. Reconnect and power-cycle

    • After flashing, unplug/replug the board and restart MEMS Studio if needed.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
MCA_DevAuthorBest answer
Associate II
Sep 9, 2026 8:05 AM UTC

Hello, thank you for your feedback.

Yes, it was indeed a connection problem, I was able to communicate directly with the sensor via I2C (with a test FW) but not through the serial port. I discovered that the NUCLEO-F401RE did not have the configuration 0R resistors SB14 and SB13 mounted so it was impossible to use the main serial communication used by MEMS Studio.

Regards,