Skip to main content
tizdipietro
Associate III
Dec 4, 2025 8:38 AM UTC
Solved

MEMS Studio MLC Debug tab not available (Version 2.2.0)

I am currently trying to build a motion detector like application using a LSM6DSV80x and it's MLC in combination with MEMS Studio (fw 2.2.0). To do so, I use the standard DataLogExtended firmware on a NUCLEO-F401RE and can successfully log and visualise data in MEMS-Studio. The MLC training can also be done successfully, and I can flash the MLC from MEMS Studio as well as use the Decision Tree Output Viewer.

But then, when I want to tweak the parameters or understand what is going on, I am missing the MLC Debug Tab in MEMS Studio (as referred to in UM3233 (MLC section) completely and cannot test on already recorded data (see picture attached).

So where can I find the Debug MLC Tab in MEMS Studio 2.2.0? If it was removed, which is the last MEMS Studio version that supports it?

(Tested both on Mac and Windows -> same issue)

 

tizdipietro_0-1764837233564.png

 

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Dec 4, 2025 9:49 AM UTC

Hi @tizdipietro ,

MLC debug is currently available only on ProfiMEMS.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Dec 4, 2025 9:49 AM UTC

Hi @tizdipietro ,

MLC debug is currently available only on ProfiMEMS.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.