Skip to main content
Associate
December 15, 2025
Question

MEMS Studio: Failed to parse log file on IR Algorithms Tuning

I'm using a STEVAL-MKI109D with the IR sensor STHS34PF80 and I need to fine tune it to detect objects with low IR emissivity, but everytime I want to load the log file into the IR Algorithm Tuning, the same error appears "Failed to parse log file". I've tried modifiying different things from the log, but everytime, I get the same error. Here is an example of a log file:

# STEVAL-MKI231KA (STHS34PF80)

time[us],t_object[LSB],t_object_comp[LSB],t_ambient[C],t_ambient_shock[LSB],t_ambient[LSB],t_ambient_shock_flag,motion[LSB],presence[LSB],presence_flag,int_1
638,-614,-614,23.470,0,2347,0,0,0,0,0
638,-671,-671,23.540,0,2354,0,0,0,0,0
729188,-641,-641,23.490,5,2349,0,0,0,0,0
1736289,-659,-659,23.440,9,2344,0,15,15,0,0
2742002,-642,-642,23.450,7,2345,0,12,12,0,0
3748506,-626,-626,23.490,2,2349,0,19,19,0,0
4754121,-617,-617,23.510,0,2351,0,30,30,0,0

Any idea on what could be happening?

4 replies

Federica Bossi
ST Technical Moderator
December 24, 2025

Hi @RVM ,

We are not able to replicate your issue. Can you please share your specific file?

Thanks!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
RVMAuthor
Associate
December 29, 2025

Hi @Federica Bossi ,

here is the file. 

Federica Bossi
ST Technical Moderator
January 14, 2026

Hi @RVM ,

Thank you!

We cannot reproduce the issue in 2.2.0. Loading the file into offline data analysis page we detected a timestamp inconsistency due to duplicated timestamp on line 4 and 5. To fix it, one of the lines shall be removed. Once done everything should work as expected.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.