Skip to main content
Echovio
Visitor II
May 5, 2026
Question

MEMS Studio AFS error with ST1VAFE3BX: magnetometer unit mismatch when using vAFE [LSB]

I am using MEMS Studio (v2.3.1) with ST1VAFE3BX to train an MLC model using AFS (Automatic Filter & Feature Selection).

My input data contains:
- 3-axis accelerometer: A_X [mg], A_Y [mg], A_Z [mg]
- vAFE channel: vAFE [LSB]

The CSV header follows the format described in AN6208:
A_X [mg], A_Y [mg], A_Z [mg], vAFE [LSB]

However, when running AFS, I get the following error:

"External sensor unit mismatch between provided external sensor name magnetometer and units LSB.
Correct units are gauss or mgauss."

This is confusing because:
- No magnetometer data is used
- Input type is set to accelerometer + vAFE
- vAFE [LSB] is consistent with ST documentation

I have already tested the following:

1. Verified CSV format (no missing values, consistent headers across all files)
2. Tested minimal dataset (only 2 CSV files)
3. Tried different headers:
- vAFE [LSB]
- vAFE_X [LSB]
- tab-separated format
4. Tested accelerometer-only input (works)
5. Tested vAFE-only input (fails)
6. Cleared workspace and settings
7. Did not reuse previous JSON configuration

The issue consistently occurs only when vAFE is included.

My questions are:

1. Does AFS in MEMS Studio 2.3.1 fully support vAFE [LSB] input for ST1VAFE3BX?
2. Is this a known issue or limitation of AFS?
3. Is there a recommended CSV format or naming convention for vAFE input?
4. Should vAFE be processed only through manual MLC configuration instead of AFS?
5. Is there a recommended MEMS Studio version that properly supports this use case?

1 reply

Federica Bossi
ST Technical Moderator
June 10, 2026

Hi ​@Echovio ,

thank you for pointing out!

We will work on this and it will be solved in the future releases.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.