Question
MEMS microphone for machine noise monitoring application to 0..10V interface
I want to implement a MEMS microphone for a machine noise monitoring application. As first I want to do some tests. My idea is to solder wires to, for example, the 'Microphone coupon board based on the MP23ABS1 analog MEMS'. Then I want to hook it up to a datalogger device which has 0..10V analog inputs.
My question is: is it possible to connect such an analog MEMS-microphone which has a 3.3V analog output, to a 0..10V input on my datalogger?