Skip to main content
reineking
Associate
August 21, 2013
Question

MEMS barometer

Posted on August 22, 2013 at 00:23

I'm using a LPS331 in a prototype. The datasheet does not give any timing information other than one can select the output data rate. What are the timing values for SPI such as max clocking frequency, etc. I search ST site and could not find any other information that would help. For I2C it says it complies with fast mode (400kHz) but nothing for SPI.

Thanks,

Tom

#mems-barometer
This topic has been closed for replies.

1 reply

Marco VENERI
ST Employee
August 23, 2013
Posted on August 23, 2013 at 16:42

Please note that this forum is specifically for MEMS Microphones and not for generic MEMS sensors. Anyhow, the LPS331AP max SPI clock frequency is 10MHz.