Skip to main content
ZZhou.11
Visitor II
May 25, 2020
Question

Mechanism of the digital temperature sensor and thermal watchdog.

I'm a studtendt from Beijing ,China. I want to use STTS75, an integrated digital temperature sensor and thermal watchdog in a high-g enviroment(~200g). Could someone tell me how the sensor works and its capabilty of bearing high acceleration? Papers about the mechnism ,design, structure and porcess are best.

​

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    May 25, 2020

    Hi @ZZhou.1​ , the STTS75 sensor (but, in general, all the temperature sensors): there is no mechanical structure (no MEMS structure, indeed) inside the T sensor package, so there is no influence of a mechanical shock on the sensor. It is basically a Delta VBE BJT based temperature sensor: I cannot share you the details of the internal architecture of the sensor since it is covered by ST confidentiality, but you can refer to the existing literature on this kind of sensors (here). Regards