Skip to main content
This topic has been closed for replies.

3 replies

Andy Saul
Associate
June 20, 2018
Posted on June 20, 2018 at 13:10

Hi Kristoffer,

I'm not aware of any settings, but there are plenty of lenses available which will exclude light in the normal spectrum and allow a passband of light that will include the 940nm wavelength required. Check '940nm ir bandpass filter' as a search on Alibaba. I have the problem now (using VL53L1X) of finding a supplier that will make a custom moulded version! If anyone reading this knows of a supplier? The company that manufactures the oval lens supplied with the VL53L1X Nucleo breakout board kit would be brilliant to talk to!

Kristoffer Gull
Associate
June 21, 2018
Posted on June 21, 2018 at 19:49

Thanks for the response i have orderet a VL53L1X Kit to see if i get more range from it. what kind of range do you get in high ambient light, outsite with the  L1X?