Skip to main content
Bill Burgess
Associate II
May 7, 2017 11:17 PM UTC
Solved

LSM9DS1 magnetometer interrupts - open-drain or push/pull?

Posted on May 08, 2017 at 01:17

The LSM9DS1 data sheet shows that the accelerometer/gyroscope module's two interrupts can be configured either as open-drain or push/pull.  However, I am missing the description of the magnetometer module's interrupt.  I assume that means it is fixed and cannot be user-configured.  Is it fixed as open-drain type, or as push/pull type?

#interrupts #lsm9ds1 #push-pull-output-or-open-drain-output
This topic has been closed for replies.
Miroslav BATEKBest answer
ST Employee
May 19, 2017 4:06 PM UTC
Posted on May 19, 2017 at 16:06

The INT_M interrupt pin is also push-pull.

3 replies

ST Employee
May 10, 2017 1:52 PM UTC
Posted on May 10, 2017 at 15:52

The DRDY_M (Magnetic sensor data ready) pin is push-pull, with active high level.

Bill Burgess
Associate II
May 10, 2017 8:12 PM UTC
Posted on May 10, 2017 at 20:12

Thanks, that helps.  But I was actually asking about the magnetometer interrupt, Pin 10, INT_M.  I couldn't find anything in the data sheet saying whether it's push-pull or open drain.  The active level (high/low) can be configured in software but not, apparently, the output type.  Do you know which it is?

Miroslav BATEKBest answer
ST Employee
May 19, 2017 4:06 PM UTC
Posted on May 19, 2017 at 16:06

The INT_M interrupt pin is also push-pull.