Skip to main content
Philip Maxwell
Associate
January 29, 2020
Question

LSM9DS1 High current usage

I am using the LSM9DS1 in our application with no problems normally. The gyro, axl and mag sensor all operating as requied. All written settings e.g. +/- range are set ok, and all registers read are giving the right outputs as device is moved around etc.

However when I try to turn the device off with the following code is still draws around 5mA all the time. I de-soldered the LSM9DS1 from one board which confirms that it is the LSM9DS1 drawing this power, even after the below commands are run.

How do I put the device to sleep? If it is not possible we will need to use an alternative device.

Have tried; 

   configureAXL(0x10,0x00); //CTRL_REG1_G (10h) power down

   configureAXL(0x20,0x00); //CTRL_REG6_XL (20h) power down 

   configureMAG(0x22,0x03);

And

   configureAXL(0x23,0x44); //CTRL_REG9 (23h) gyro sleep 

   configureAXL(0x10,0x00); //CTRL_REG1_G (10h) power down

   configureAXL(0x20,0x00); //CTRL_REG6_XL (20h) power down 

   configureMAG(0x22,0x03);

Thanks

Phil

    This topic has been closed for replies.

    1 reply

    Philip Maxwell
    Associate
    February 1, 2020

    Issue was that the MCU connected to the device had an internal pull-up enabled which was drawning a lot of current for some reason.