Skip to main content
Associate
Dec 18, 2024 4:49 PM UTC
Solved

LSM9DS1 Gyroscope/Accelerometer Data ready interrupt not working

I am trying to get the an values ready interrupt working, but I cannot seem to find the right configuration of registers. Normal threshold interrupts are working as expected.

After the normal setup and using all different speeds ODR, when setting INT1_CTRL to INT_DRDY_XL active, I do not get any interrupts. The oscilloscope shows no change as well on either H_LACTIVE as well. Is there a sample that can be provided which has a working implementation of the interrupt working? So far all public sources have non working code. 

As an MCU I am using an ESP32 and Arduino.

Here is my current initialisation:


// Enable accelerometer
writeRegister(0x1F, 0x38); // CTRL_REG5_XL - Enable XYZ axes
writeRegister(0x20, 0x60); // CTRL_REG6_XL - ODR 952 Hz

// Set up interrupt generator and DRDY
writeRegister(INT1_CTRL, 0x01); // Enable IG_XL (bit 6) and DRDY_XL (bit 0)
writeRegister(CTRL_REG8, 0x00); // Active HIGH, push-pull

 

This topic has been closed for replies.
schartnercBest answer
Associate
Jan 3, 2025 7:41 AM UTC

Thank you for the answer. The internet did not provide any working example. 

Thanks for the quick answer!

2 replies

Peter BENSCH
ST Technical Moderator
Dec 19, 2024 5:41 PM UTC

Welcome @schartnerc, to the community!

Unfortunately, the LSM9DS1 was discontinued some time ago, so that no more information is officially available. If you can't find anything in the depths of the never-forgetting internet, probably nobody will be able to help you.

I am extremely sorry not to be able to help you.

Regards /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
schartnercAuthorBest answer
Associate
Jan 3, 2025 7:41 AM UTC

Thank you for the answer. The internet did not provide any working example. 

Thanks for the quick answer!