Skip to main content
Damon Kelly
Associate II
February 20, 2019
Question

LSM9DS1 DRDY_M and DEN_A/G pins

How do the LSM9DS1 DRDY_M and DEN_A/G pins function?

    This topic has been closed for replies.

    6 replies

    Damon Kelly
    Associate II
    February 20, 2019

    I see this has been answered before.

    However, how should DEN_A/G be connected? Gnd, Vdd, floating?

    Eleon BORLINI
    ST Employee
    February 20, 2019

    Hi Damon, you can connect DEN_A/G pin to your MCU without initializing it, if you don't need to use it.

    Damon Kelly
    Associate II
    February 26, 2019

    If I'm not using it, should I connect it to GND or Vdd?

    Eleon BORLINI
    ST Employee
    February 28, 2019

    Hi Damon, yes, connecting to GND should be ok

    Damon Kelly
    Associate II
    March 1, 2019

    Thank you, Eleon

    NHend.7
    Associate II
    March 10, 2019

    Hi from my understanding that DEN is a I/O pin that creates a trigger to Automatically send data to the MCU. This can be used instead of a standard i2c or spi call?

    This pin seems very dangerous as there is very very little info on how to use it correctly.

    So grounding this pin is for the best until the documentation is updated.

    BR