Skip to main content
Associate III
Apr 15, 2026 12:33 PM UTC
Solved

LSM6DSV320X sensor not responding

Hello everyone. 

I would really appreciate if someone could help me sort out a really annoying issue i have with a new STM32WB5MMGH6 based board i made.

On this board i have two sensors connected to the same SPI interface (hspi2) with different CS pins to address the sensors. Here's the schematic sections of the two sensors : 

MS5607 : 

Screenshot 2026-04-15 at 14.24.40.png

 

LSM6DSV320XTR with an auxiliary IIS2MDCTR tied directly to it (for the test board, the magnetometer is not soldered yet):

Screenshot 2026-04-15 at 14.25.41.png

I'm currently on test phase, and the MS5607 is responding correctly. But the LSM6DSV320XTR does not respond at all. i'm not even getting the whoami ID (i get a 0).

For the SPI configuration i have this : 

Screenshot 2026-04-15 at 14.29.50.png

For the 2 Chip Select pins i have this config : 

Screenshot 2026-04-15 at 14.31.57.png

Screenshot 2026-04-15 at 14.31.57.png

 

I don't understand where the problem comes from. Could someone help me asap ? I'm losing hope :(

yaxsomoBest answer
Associate III
Apr 22, 2026 1:06 PM UTC

Hello @Federica Bossi , I finally found the issue. It was a solder joint issue, and i blamed the software for nothing. One tip for other users that may encounter similar issues : When hand soldering a sensor like this one with a hot air gun, first apply solder on the PCB pads, then apply solder ALSO on the sensor. I applied solder on PCB pads but not on the sensor, resulting in really poor connection and therefore, a unusable IC. 

Thank you for helping, I'm closing the thread

3 replies

Federica Bossi
ST Technical Moderator
Apr 20, 2026 8:57 AM UTC

Hi @yaxsomo ,

Using MKI109D motherboard with STEVAL-MKI251A, the sensor communicate correctly using your SPI configuration (Baud Rate: 4MBits/s, CPOL: High, CPHA: 2Edge) and assuming IMU_CS configuration same of BARO_CS that you posted.

Debug tips:

Are you sure that SPI2 lines are connected to LSM6DSV320X? Do they move on its side when communicate with the other sensor (oscilloscope probing)?

Did you check on IMU_CS behavior (oscilloscope probing)?

In your main FW when LSM6DSV320X communication takes place? Did you try to communicate only with it?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yaxsomoAuthor
Associate III
Apr 21, 2026 10:50 PM UTC

Hello @Federica Bossi , sorry for the late response, i'm trying to debug this thing.
I'm starting to think it's a soldering issue, because when communicating with the barometer, there's no issue.

And the LSM6DSV320X is soldered with a hot air gun. 

I tried to communicate only with the IMU on main.c and i get zeroed values, which is not good at all.

Is it an issue if the sensor is powered (both VDD and VDDIO) with 3.3V ? 

yaxsomoAuthorBest answer
Associate III
Apr 22, 2026 1:06 PM UTC

Hello @Federica Bossi , I finally found the issue. It was a solder joint issue, and i blamed the software for nothing. One tip for other users that may encounter similar issues : When hand soldering a sensor like this one with a hot air gun, first apply solder on the PCB pads, then apply solder ALSO on the sensor. I applied solder on PCB pads but not on the sensor, resulting in really poor connection and therefore, a unusable IC. 

Thank you for helping, I'm closing the thread