Skip to main content
Associate
August 28, 2024
Solved

LSM6DSV16X FIFO batch data rate

In high-accuracy ODR mode, can the frequency of writing to the fifo be automatically aligned,

for example 960 to 1000hz

fluchc_0-1724837138350.png

fluchc_1-1724837142546.png

 

 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
August 29, 2024

Hi @fluchc ,

The FIFO rate is always aligned to the ODR or its submultiples. If you put 1000 Hz and BATCH_RATE = 960 Hz then BATCH_RATE will also be 1000 Hz. If for example ODR = 1000 Hz and BATCH_RATE is 480 Hz then the real batch_rate is 500 Hz.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
August 29, 2024

Hi @fluchc ,

The FIFO rate is always aligned to the ODR or its submultiples. If you put 1000 Hz and BATCH_RATE = 960 Hz then BATCH_RATE will also be 1000 Hz. If for example ODR = 1000 Hz and BATCH_RATE is 480 Hz then the real batch_rate is 500 Hz.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
fluchcAuthor
Associate
August 29, 2024

thanks