Skip to main content
Associate
Jan 16, 2025 2:30 PM UTC
Question

LSM6DSV16X accelerometer settings for low noise readout for small movements

I want to recognise small movements with small acceleration.

Which mode is best suited?

Is it better to have a high sampling rate or a lower one?

which filters?

where do the large peaks (incorrect values) come from?

But I can already recognise the acceleration and braking

This topic has been closed for replies.

8 replies

Federica Bossi
ST Technical Moderator
Jan 16, 2025 4:13 PM UTC

Hi @Stefan3 ,

A smaller FS range (e.g., ±2g) will provide higher sensitivity and better resolution for detecting small accelerations.

A higher sampling rate can capture more data points and provide a more detailed representation of the movement. This is useful for detecting small and rapid changes in acceleration. However, it will also increase power consumption and the amount of data to process.

I suggest you to use High-accuracy ODR (HAODR) mode. This mode typically offers better precision and lower noise.

About the incorrect values, did you enable the BDU bit?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Stefan3Author
Associate
Jan 17, 2025 2:09 PM UTC

Hi Federica

±2g is set.

I haven't done anything yet
except set CTRL1(10h) to 960Hz and read with 10mSec (100Hz) with the I2C bus (1MHz).

I have enough power available but reading faster than 100Hz is not so easy.

Should I choose low-power mode3 (8mean)? Or a high performance mode?

Should I enable the BDU bit anyway?

2025-01-17_14-54-46.PNG

 

Federica Bossi
ST Technical Moderator
Jan 17, 2025 2:25 PM UTC

Hi @Stefan3 ,

Yes, it is always suggested to enable the BDU bit.

In addition, high performance mode is suggested for this kind of application :)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.