Skip to main content
Deepak.Aagri
Associate III
October 4, 2021
Question

LSM6DSOX (steval-mki178v2) i2c driver for P-NUCLEO-WB55

Hello ST,

I am using LSM6DSOX sensor and P-NUCLEO-WB55 Board for tilt and motion sensing. I didn't get any basic example or libraries to interface LSM6DSOX with P-NUCLEO-WB55 Dongle board.

I tried with basic way for SPI and I2c communication but unfortunately didn't get success.

It is my humble request to you Please provide the some basic tested example for LSM6DSOX with P-NUCLEO-WB55 board. So we can rapidly develop our product.

Note- Below given link 10K pull up resistor connected at SCL and SDA pin

https://www.mouser.in/datasheet/2/389/steval-mki178v2-1848661.pdf

Best Regards

Deepak Aagri

This topic has been closed for replies.

1 reply

TBomb.1
Visitor II
October 7, 2021

Hi, maybe the FP-SNS-MOTENVWB1 function pack can help you. It embeds sample implementation that are available for the X-NUCLEO-IKS01A3 connected to a P-NUCLEO-WB55. The X-Nucleo board supports the LSM6DSO(X) device, or in any case you can plug the dil24 adapter you mentioned on it.

https://www.st.com/en/embedded-software/fp-sns-motenvwb1.html

https://www.st.com/en/ecosystems/x-nucleo-iks01a3.html

\Tom