Skip to main content
Associate
Mar 10, 2025 7:07 AM UTC
Question

LSM6DSOX MLC ActivityStates

Hi Team, 

We are working with the LSM6DSOX sensor and integrating it with two different MCUs: nRF5340 and ATSAMD51, using the I2C communication protocol. We have been able to successfully read the device ID, accelerometer data, and gyroscope data. Additionally, we've implemented our own logic for step detection and step counting.

Recently, we learned about the Machine Learning Core (MLC) feature, which provides useful capabilities like detecting activity states (idle, walk, run). We obtained the .ucf file for MLC, used the UNICO tool to generate the corresponding .h file, and attempted to integrate it into our application. We followed the documentation and tried monitoring the MLC_STATUS (0x70) register to track activity states.

Challenges faced:

  1. First Attempt with nRF5340 MCU: Initially, we tested the MLC functionality with the nRF5340 MCU using I2C communication. However, when we read the MLC_STATUS register, we consistently received 0x00, no matter the movement or activity. Despite testing different motions, there were no changes in the register output.

  2. Currently Testing with ATSAMD51 MCU: After facing the issue with the nRF5340, we decided to try the same MLC configuration with the ATSAMD51 MCU. After writing the generated .h conf file to the device using i2c_burst_write, we continuously monitor the MLC_STATUS (0x70) register. However, we consistently receive a value of 0x02, even when there is no movement or when attempting to walk or run. The value remains unchanged, which suggests that the activity state isn’t being updated correctly.

We would greatly appreciate any guidance or troubleshooting steps to resolve this issue, particularly in regard to:

Proper configuration of the MLC functionality on both MCUs.

The correct sequence of operations for initializing and monitoring the MLC_STATUS register.

Any additional steps or considerations to ensure the MLC feature works as expected on both platforms.

Thanks,
Ilam

1 reply

Federica Bossi
ST Technical Moderator
Dec 24, 2025 9:01 AM UTC

Hi @Ilamparithi ,

To properly use the LSM6DSOX Machine Learning Core (MLC), ensure the following steps:

  1. Reset the sensor and configure the accelerometer’s ODR and full scale according to MLC requirements (e.g., 26 or 52 Hz, 2g or 4g).
  2. Enable access to embedded functions memory (FUNC_CFG_ACCESS), then write the MLC configuration from the .h file to the device.
  3. Disable FUNC_CFG_ACCESS and enable the MLC engine.
  4. Clear any interrupt flags before starting to monitor the MLC_STATUS register.
  5. Read the MLC_STATUS register with a delay matching the accelerometer ODR, allowing the MLC engine time to update.
  6. Optionally configure interrupt routing for MLC events.

Also, verify I2C communication reliability and ensure timing/delays are adequate on both MCUs.

Let me know if this helps.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.