Skip to main content
Associate II
Oct 23, 2025 1:16 AM UTC
Solved

LSM6DSO temperature on working mode

Dear Sir,

Our project using LSM6DSO IMU to detect the position, the sensor temperature is very high after power on and Initialization, it's over 80 degree, I think it's abnormal, I attach the sch, can you give some suggestions, thanks a lot.

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 28, 2025 3:08 PM UTC

Hi @Jali ,

No, if INT2 is not used, leave it floating or connect it to ground through a resistor as per datasheet recommendations.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

Federica Bossi
ST Technical Moderator
Oct 23, 2025 2:40 PM UTC

Hi @Jali ,

I confirm you that such a temperature value is abnormal. Here are some suggestions:

  • Ensure the sensor is powered at the correct voltage (typically 1.8 V for LSM6DSO). Overvoltage can cause excessive power dissipation and heating.
  • Ensure no shorts or wiring mistakes on the I2C lines or chip pins that could cause excessive current draw.
  • Start with the sensor in low-power or power-down mode and verify temperature behavior before enabling full operation.
  • Use an IR thermometer or thermal camera to confirm the actual sensor temperature.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
JaliAuthor
Associate II
Oct 24, 2025 12:14 AM UTC

Hi  Federica,

we connect the INT2 pin to vcc directly, is it right?

 

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 28, 2025 3:08 PM UTC

Hi @Jali ,

No, if INT2 is not used, leave it floating or connect it to ground through a resistor as per datasheet recommendations.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.