Associate III
Jan 24, 2019 10:17 AM UTC
Question
LSM6DSO SPI communication problem
- 13 replies
- 3539 views
Good morning,
I am trying to read the WHO_AM_I register from LSM6DSO, but it doesn't respond as needed. I will attach a picture from signal analyzer (D0 is CS, D1 is CLK, D2 is MISO, D3 is MOSI). It looks like its respond is 0x50 instead of 0x6C. What should I change?
I tried with a MAX32630 and it was working (8 bits transfer mode).
When I try with RS14100 (16 bits mode) it responds with 0x50 instead of 6C.
Gabriel