Skip to main content
Associate
Jun 23, 2026 7:49 AM UTC
Solved

LSM6DSO Pins 10 and 11

Hello, we are planning to use LSM6DSO in Mode 1, but PCB is fixed and pins 10 and 11 are connected to GND. This conflicts with LSM6DSO datasheet but I was wondering if it is still OK to connect them to GND. Can you clarify on this?

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jul 2, 2026 7:32 AM UTC

Hi ​@Tatmaz ,

For LSM6DSO Mode 1, pins 10 (OCS_Aux) and 11 (SDO_Aux) are not meant to be tied to GND.
According to the datasheet, pin 10 should be left unconnected, and pin 11 should be left unconnected or tied to VDDIO.
So if your PCB has these pins hard-wired to GND, it is not the recommended configuration and behavior is not guaranteed by ST.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jul 2, 2026 7:32 AM UTC

Hi ​@Tatmaz ,

For LSM6DSO Mode 1, pins 10 (OCS_Aux) and 11 (SDO_Aux) are not meant to be tied to GND.
According to the datasheet, pin 10 should be left unconnected, and pin 11 should be left unconnected or tied to VDDIO.
So if your PCB has these pins hard-wired to GND, it is not the recommended configuration and behavior is not guaranteed by ST.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
TatmazAuthor
Associate
Jul 21, 2026 8:30 AM UTC

Hi Federica,

 

Thank you for the answer. I am confused about one thing, you suggested that connecting pins 10 and 11 to GND is not a problem for LSM6DSV320X in the topic below, is it problematic only for LSM6DSO?