Skip to main content
CWang_221
Visitor II
August 2, 2021
Question

LSM6DSO issues with I3C

LSM6DSO will NACK the broadcast after the RSTDAA sent in the reboot probe sequence.

Here is the case to reproduce the issue:

1. Only one LSM6DSO is on the I3C bus which is in pure I3C mode.

2. The first-time kernel boot after power-up is okay. I3C bus and LSM6DSO both probe okay.

3. Execute command “reboot�? in rootfs to do the warm reset.

4. The LSM6DSO will NACK the second I3C bus broadcast after I3C sends the broadcast of RSTDAA(0x6) when it is rebooting. 

0693W00000D1F4WQAV.pngIs there anyone meet this problem? I use the upstreamed code of this sensor in Linux kernel: drivers/iio/imu/st_lsm6dsx/st_lsm6dsx_i3c.c

Thanks.

This topic has been closed for replies.

2 replies

DSull.3
Visitor II
August 23, 2021

Hi, I know that ST supports also on Github for specific drivers-related topics:

https://github.com/torvalds/linux/blob/master/drivers/iio/imu/st_lsm6dsx/st_lsm6dsx_i3c.c

You can try to open an issue there to get more help from Linux community.

\Dk

Javier1
Principal
August 23, 2021

@CWang_221​  You just introduced me to i3c, thanks

hit me up in https://www.linkedin.com/in/javiermuñoz/