Skip to main content
BNewl.1
Associate
Sep 4, 2020 2:46 PM UTC
Solved

LSM6DSO degrees per second full scale calculation

In the datasheet, it says the gyroscope in the LSM6DSO is 1LSb = 70 mdps at +/-2000 dps full scale. I'm curious how this is obtained. For a signed 16-bit number I get 2000 / 32768 = 61mdps.

For the accelerometer, 1LSb = 0.061 mg at +/- 2g full scale, which I agree with. 2 / 32768 = 0.061 mg.

Where does the discrepancy come from in my gyroscope calculation? Is it simply that the gyroscope is not sensitive enough to realize the ideal angular rate precision?

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Sep 9, 2020 12:06 PM UTC

    Hi @BNewl.1​ ,

    basically yes, you are right: the gyro LSB is physically limited to 70mdps.

    You can refer to lsm6dso_reg.c for the C code implementation of the LSB to physical units conversion.

    -Eleon

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Sep 9, 2020 12:06 PM UTC

    Hi @BNewl.1​ ,

    basically yes, you are right: the gyro LSB is physically limited to 70mdps.

    You can refer to lsm6dso_reg.c for the C code implementation of the LSB to physical units conversion.

    -Eleon