Skip to main content
BNall.1
Associate
February 28, 2022
Solved

LSM6DSO: Are the accel and gyro biases sensitive to temperature variations? The data sheet only talks about the "sensitivity change vs temperature" which indicates an impact on LSB size (resolution change), however, may I know the impact on bias valu

..

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
March 4, 2022

Hi @BNall.1​ ,

please consider that the bias (named LA_OffDr and G_OffDr) variations versus temperature are available in the datasheet, p.9:

0693W00000KbRlIQAV.pngIt is an average variation, that typically increases in both direction(cooling and heating) from the reference 25°C.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon

4 replies

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
March 4, 2022

Hi @BNall.1​ ,

please consider that the bias (named LA_OffDr and G_OffDr) variations versus temperature are available in the datasheet, p.9:

0693W00000KbRlIQAV.pngIt is an average variation, that typically increases in both direction(cooling and heating) from the reference 25°C.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon

BNall.1
BNall.1Author
Associate
March 10, 2022

Hi @Eleon BORLINI​ , thanks for the answer. Is this bias variation over temperature spec applicable after applying temperature-based bias compensation, or is this a measurement of the sensor HW variation without any explicit compensation?

BNall.1
BNall.1Author
Associate
March 10, 2022

Is it also true that accelerometer (spec force) and gyro sensor measurement noise (std dev) is not temperature dependent?