Solved
Eleon BORLINIBest answer
ST Employee
June 11, 2020
Uhm... so basically the temperature increases correctly but it is always 4/5°C below the effective ambient temperature, right? For example, if outdoor is 34°C, the sensor will read 30°C? and same for negative temperatures?
Please note that the Toff (the temperature offset, is declared to be between -15°C and +15°C, so 4/5°C falls in this range. If your offset is constant, you can add it to your Temperature data via SW and apply it to all the temperature range of your interest.
Regards