Skip to main content
SWood.5
Associate II
October 31, 2018
Question

LSM6DSL: Why isn't the gyroscope data appearing in the FIFO?

I am trying to use the FIFO to store accelerometer and gyroscope data on the LSM6DSL. While the acceleration data appears correctly in the FIFO, the gyroscope x and y axis data is only being stored as zeros. The gyroscope z axis data is being stored correctly in the FIFO, however. Additionally, when I read the gyroscope x and y axis registers directly, they appear correct. The FIFO_CRTL3 register is set to include both the acceleration and angular rate data in the FIFO without decimation. Any ideas what is happening? I have looked through the datasheet and application note extensively. Thank you!

    This topic has been closed for replies.

    6 replies

    ST Employee
    October 31, 2018

    Can you share your sensor configuration?

    SWood.5
    SWood.5Author
    Associate II
    October 31, 2018

    The following is our sensor configuration. We also have low pass filters enabled and timestamps stored in the FIFO, so I included those register configurations too, in case they have any affect.

    //Power managment

    CTRL7_G = 0b0

    CTRL6_C = 0b10000011

    //FIFO Config

    CTRL3_C = 0b01000100

    MASTER_CONFIG = 0b0

    WAKE_UP_DUR = 0b00010000

    CTRL10_C = 0b00110100

    MD1_CFG = 0b1

    FIFO_CTRL5 = 0b00110100

    FIFO_CTRL = 0b00111001

    FIFO_CTRL2 = 0b10000000

    FIFO_CTRL3 = 0b00001001

    FIFO_CTRL4 = 0b00001000

    INT1_CTRL = 0b11

    //Gyro and Accel Config

    CTRL4_c = 0b00001010

    CTRL2_G = 0b01111100

    CTRL8_G = 0b0

    CTRL1_XL = 0b01111110

    //Timestamp start

    TIMESTAMP2_REG = 0xAA

    Thank you very much!

    ST Employee
    November 2, 2018

    Can you please set the FIFO ODR to maximum 6.66kHz in the FIFO_CTRL5 register.

    if you need lower data rate in FIFO please set the decimation.

    SWood.5
    SWood.5Author
    Associate II
    November 2, 2018

    I set the FIFO ODR to maximum, and set the appropriate decimation rate, but I am still getting zeros for the gyro x and y.

    ST Employee
    November 5, 2018

    It is strange, can you check the content of the FIFO_PATTERN_[9:0] bits in the FIFO_STATUS3 and FIFO_STATUS4 registers, to see if there are accelerometer and gyro data.

    0690X000006CJRbQAO.png

    SWood.5
    SWood.5Author
    Associate II
    November 5, 2018

    I checked the FIFO pattern, and the accelerometer and gyro data are included. However, when I check the gyro x and gyro y registers directly now, I also get zeros. So there may be something wrong with the gyro configuration? My apologies for not catching that earlier.