Skip to main content
stefan schoenbauer
Associate
January 18, 2018
Question

LSM6DSL. Wake-Up Interrupt

Posted on January 18, 2018 at 09:07

I have configured the Wake-Up interrupt (with highpass filter) as described in the application note:

1. Write 60h to CTRL1_XL // Turn on the accelerometer // ODR_XL = 416 Hz, FS_XL = 2 g

2.Write 90h to TAP_CFG // Enable interrupts and apply high-pass digital filter; latched mode disabled

3.Write 00h to WAKE_UP_DUR  // No duration

4.Write 02h to WAKE_UP_THS // Set wake-up threshold

5.Write 20h to MD1_CFG // Wake-up interrupt driven to INT1 pin

All other registers are used with default values.

After 2.6 ms of writing the MD1_CFG register the INT1 pin gets high and remains high 50 ms. I would expect, that the pin gets hight after a wake-up event occurs.. This case happens independently of the sampling frequency, wakeup trheshold or wakeup duration. After the 50 ms it seems to  work fine.

I expect that the signal on INT1 is low until an wake-up event.  Is this the normal behavior or or did I misconfigure something?

#lsm6dsl #wake-up
This topic has been closed for replies.

1 reply

ST Employee
January 18, 2018
Posted on January 18, 2018 at 15:11

I'm not able to replicate this issue.

Are you sure the signal is generated by the LSM6DSL?

Can you please share the part of the code when it happened?